Hardware requirements

  • Micro USB cable

  • EVK-MIMXRT595

  • Personal Computer

Board settings

To make i2c example work, connections needed to be as follows: I2C11 connected to I2C12 SCL P4_21(J28 pin10) –> P5_1(J28 pin4) SDA P4_22(J28 pin9) –> P5_0(J28 pin3)

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J40) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.