Hardware requirements

  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output in the terminal window:

 GPIO Driver example

 The LED is taking turns to shine.

 Standard port read: 2018004

 Masked port read: 2010000

 Port state: 18004

 Port state: 18004
 ...

Press the SW2 will toggle the LED BLUE state.