Hardware requirements
Mini USB cable
Two FRDM-K22F boards
Personal Computer
Board settings
SPI one board: Transfer data from one instance to anther instance on the other board. Note: Please separate the connected wires(CLK wire is important), if not, mixed wires may caused electromagnetic interference and data will transfer error.
Master Board Slave Board
INSTANCE0(SPI0) CONNECTS TO INSTANCE1(SPI1)
Pin Name Board Location Pin Name Board Location
SIN J1 pin 11 SOUT J1 pin 16
SOUT J1 pin 16 SIN J1 pin 11
SCK J1 pin 15 SCK J1 pin 15
PCS0 J24 pin 9 PCS0 J24 pin 9
GND J2-14 GND J2-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
This is DSPI half-duplex polling transfer example!
SPI master board will transmit data to slave board first, then receive data from slave board.
To make sure the transfer work successfully, please start the slave board first!
Besides, Master will transfer data by polling way, and slave will use interrupt way.
Master start to tansfer data...
The received data are:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
DSPI half-duplex transfer all data matched!