Hardware requirements

  • Mini/micro USB cable

  • FRDM-K32L2A4S board

  • Personal Computer

Board settings

  • Connect input signal to J2-6

Prepare the Demo

  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see information from the terminal as below.

TPM dual-edge capture example

Once the input signal is received the input capture values are printed

The input signal's pulse width is calculated from the capture values & printed

Capture value C(n)V=0

Capture value C(n+1)V=26d4

Input signals pulse width=82 us