Hardware requirements

  • Mini/Micro USB cable

  • FRDM-K32L2B board

  • Personal Computer

Board settings

FXOS8700 must be available on board to run this example. If it’s not soldered, the example cannot work.

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as shown below.

Welcome to the BUBBLE example

You will see the change of angle data and LED brightness when change the angles of board

x= 6 y = 22 x= 8 y = 26 x= 10 y = 28 x= 10 y = 28 x= 11 y = 29 x= 11 y = 29