Hardware requirements

  • Mini USB cable

  • FRDM-K32L2B board

  • Personal Computer

Board settings

Connect J4-2(PTB0/ADC0_SE8) to J4-11(PTE30/DAC0_OUT)

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Download the program to the target board.

  3. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

  4. Run “run.py” on your PC with -p (–port) parameter to select COM port (baud rate can be also set through -b (–bd) parameter).

For detailed instructions, see the appropriate board User’s Guide.

Running the demo

A. Server on the board, client on the PC:

Selected UART port: com15, 115200 bd eRPC server has been run eRPC client has been created Board configuration: DAC: True LED: Red=True, Green=True, Blue=True ADC configuration: Vref=3.29999995232 V Atomic steps=4096.0


eRPC Remote Control example

-> Press ‘1’ for DAC-ADC conversion -> Press ‘2’ for GPIO LED -> Press ‘3’ for Accelerometer and Magnetometer values 2 Select which LED should be turned on: –> Press ‘1’ for red –> Press ‘2’ for green 1


eRPC Remote Control example

-> Press ‘1’ for DAC-ADC conversion -> Press ‘2’ for GPIO LED -> Press ‘3’ for Accelerometer and Magnetometer values 3 Read value from Accelerometer and Magnetometer: Accelerometer axis: x=7608, y=16736, z=-512 Magnetometer axis: x=0, y=0, z=0


eRPC Remote Control example

-> Press ‘1’ for DAC-ADC conversion -> Press ‘2’ for GPIO LED -> Press ‘3’ for Accelerometer and Magnetometer values 1 Enter voltage <0V - 3.3V>: 1.5 DAC is set for 1.5 V which is 1861 of atomic steps ADC value: 1.50095212675 V

B. Server on the PC, client on the board:

[Message from board] Button SW1 was pressed [Message from board] Button SW3 was pressed