Hardware requirements
Micro USB cable
Two FRDM-K32L3A6 boards
Personal Computer
Board settings
To make lpi2c example work(M4), connections needed to be as follows:
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C1_SCL J1-10(PTB14) LPI2C1_SCL J1-10(PTB14)
LPI2C1_SDA J2-6(PTB6) LPI2C1_SDA J2-6(PTB6)
GND J2-14 GND J2-14
To make lpi2c example work(M0), connections needed to be as follows:
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C3_SCL J3-15(PTB15) LPI2C3_SCL J3-15(PTB15)
LPI2C3_SDA J3-13(PTB16) LPI2C3_SDA J3-13(PTB16)
GND J2-14 GND J2-14
Prepare the Demo
Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for JLink serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following message shows in the terminal if the example runs successfully.
LPI2C board2board polling example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .