Hardware requirements
Mini/Micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
Using instance 1 of LPUART interface to transfer data to itself. TX pin is connected with RX pin.
LPUART1 CONNECTS TO LPUART1
Pin Name Board Location Pin Name Board Location
TXD J1-4 RXD J1-2
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
USART 9-bit mode example begins
USART is configured with address, only data sent to itself after matched address can be received
USART will send first piece of data out:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
USART will address itself
USART will send the other piece of data out:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
USART received data:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
All data matches!