Hardware requirements

  • Micro USB cable

  • FRDM-KE15Z board

  • USB to Com converter

  • Personal Computer

Board settings

This example requires connecting the FLEXIO pins with the USB2COM pins The connection should be set as following: - PTE11, FLEXIO_UART_RX_PIN, J2-15 - PTE10, FLEXIO_UART_TX_PIN, J2-17 - GND , J2-14

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

  • 115200 baud rate

  • 8 data bits

  • No parity

  • One stop bit

  • No flow control

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

FLEXIO UART RX ring buffer example
Send back received data
Echo every 8 bytes