Hardware requirements
Micro USB cable
FRDM-KE16Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TSI_V5 Self-Cap mode Example Start!
Calibrated counters for channel 0 is: 65535
Calibrated counters for channel 1 is: 65535
Calibrated counters for channel 2 is: 65535
Calibrated counters for channel 3 is: 65535
Calibrated counters for channel 4 is: 65535
Calibrated counters for channel 5 is: 65535
Calibrated counters for channel 6 is: 65535
Calibrated counters for channel 7 is: 65535
Calibrated counters for channel 8 is: 523
Calibrated counters for channel 9 is: 65535
Calibrated counters for channel 10 is: 65535
Calibrated counters for channel 11 is: 65535
Calibrated counters for channel 12 is: 65535
Calibrated counters for channel 13 is: 65535
Calibrated counters for channel 14 is: 65535
Calibrated counters for channel 15 is: 553
Calibrated counters for channel 16 is: 65535
Calibrated counters for channel 17 is: 1908
Calibrated counters for channel 18 is: 1936
Calibrated counters for channel 19 is: 65535
Calibrated counters for channel 20 is: 2084
Calibrated counters for channel 21 is: 45421
Calibrated counters for channel 22 is: 65535
Calibrated counters for channel 23 is: 65535
Calibrated counters for channel 24 is: 65535
NOW, comes to the software trigger scan using polling method!
Channel 0 Normal mode counter is: 65535
Channel 1 Normal mode counter is: 65535
NOW, comes to the software trigger scan using interrupt method!
Channel 0 Normal mode counter is: 65535
Channel 1 Normal mode counter is: 65535
NOW, comes to the hardware trigger scan method!
After running, touch pad E1 each time, you will see LED toggles.