Hardware requirements

  • Micro USB cable

  • Two FRDM-KE17Z boards

  • Personal Computer

Board settings

LPI2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C0 pins of MASTER_BOARD are connected with LPI2C0 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name     Board Location     Pin Name     Board Location
LPI2C0_SCL   J2-18              LPI2C0_SCL   J2-18
LPI2C0_SDA   J2-20              LPI2C0_SDA   J2-20
GND          J2-14              GND          J2-14

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS LPI2C board2board interrupt example -- Master transfer.
Master will send data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7  
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f  
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f  

Receive sent data from slave :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7  
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f  
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f  


End of LPI2C example .