Hardware requirements
Micro USB cable
FRDM-KE17Z board, FRDM-TOUCH board
Personal Computer
Board settings
Keep the default configuration for the FRDM board and connect the FRDM-TOUCH board with the FRDM board.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When running successfully, LED will be turned on when the electrode on FRDM-TOUCH board is touched and the LED will be turned off after the electrode is released. The log output in terminal shall be similar as below:
TSI mutual mode demo.
TSI key touched.
TSI key released.
TSI key touched.
TSI key released.