Hardware requirements
Micro USB cable
FRDM-KE17Z board
Personal Computer
Board settings
The flexio_i2c_read_accel_value example is requires connecting the FLEXIO pins with the I2C pins of accelerometer The connection should be set as following: FLEXIO_I2C connected to LPI2C0 SDA PTA11(J2-17) –> PTA16(J2-18)
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
FlexIO I2C example read accelerometer value
Found a FXOS8700 on board, the device address is 0x1C.
The accel values:
status_reg = 0xff , x = 511 , y = -66 , z = 2065
status_reg = 0xff , x = 509 , y = -70 , z = 2054
status_reg = 0xff , x = 513 , y = -64 , z = 2064
status_reg = 0xff , x = 514 , y = -71 , z = 2064
status_reg = 0xff , x = 508 , y = -67 , z = 2066
status_reg = 0xff , x = 512 , y = -62 , z = 2060
status_reg = 0xff , x = 514 , y = -73 , z = 2060
status_reg = 0xff , x = 511 , y = -64 , z = 2056
status_reg = 0xff , x = 518 , y = -68 , z = 2064
status_reg = 0xff , x = 507 , y = -67 , z = 2066
End of I2C example .