Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Board settings
This example project uses ACMP instance 0 to compare the voltage signal input from channel 0(J5-1) with the voltage signal(half of VDDA) output by ACMP’s internal DAC. In order to observe the low power wakeup phenomenon, channel 0(J5-1) should be connected to GND signal(J2-14) on the board before the example running. Example will exit stop mode when channel 0(J5-1) is disconnected from GND signal and the disconnected time is last for about 1s.
Prepare the Demo
Connect a USB cable between the PC host and the MCU-LINK USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
${ANCHOR}