Hardware requirements
Micro USB cable
FRDM-KE17Z512 board
An oscilloscope
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
FTM example to output PWM on 2 channels
You will see a change in LED brightness if an LED is connected to the FTM pin
If no LED is connected to the FTM pin, then probe the signal using an oscilloscope