Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXA153 board. FRDM-MCXA153 UART pins:
TX of USB2COM to J2-4(P3_14)
RX of USB2COM to J2-2(P3_15)
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
7 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
Lpuart interrupt example with seven data bits
Board receives 8 characters then sends them out
Now please input: