Hardware requirementsο
FRDM-MCXA153 board
USB-C cable
Personal Computer
Board settingsο
No special HW settings.
Board specific example notesο
In case of this board MCUBoot si configured for OVERWRITE_ONLY
image strategy.
This means that an image in the secondary slot is simply moved to the primary slot
by overwriting the current version. This means that itβs not possible to revert
back to previous version once the new image is installed.