Hardware requirements
Type-C USB cable
FRDM-MCXA156 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the CTimer simple match demo using interrupts in the terminal window:
CTimer match example to toggle the output.
This example uses interrupt to change the match period.
You can see the red led and blue led will blinking alternating frequently and then return to the original status.