Hardware requirements
Type-C USB cable
FRDM-MCXA156 Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
SLAVE(FlexIO SPI) connect to MASTER(LPSPI0)
Pin Name Board Location Pin Name Board Location
SOUT J8 pin 14 SIN J6 pin 5
SIN J8 pin 13 SOUT J6 pin 6
SCK J8 pin 15 SCK J6 pin 4
PCS0 J8 pin 16 PCS0 J6 pin 3
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J21.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
LPSPI Master interrupt - FLEXIO SPI Slave interrupt example start.
This example use one lpspi instance as master and one flexio spi slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- FLEXIO_SPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is FLEXIO SPI slave call back.
LPSPI master <-> FLEXIO SPI slave transfer all data matched!
End of Example.