Hardware requirements

  • Type-C USB cable

  • FRDM-MCXL255 Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB Type-C cable between the host PC and the LPC-Link USB port (P6) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, will get the similar messages on the terminal.

TRDC example start
Set the MBC selected memory block not accessiable
Resolve access error
The MBC selected block is accessiable now
TRDC example Success