Hardware requirements
Mini USB cable
USB to TTL converter
FRDM-MCXC242 board
Personal Computer
Board settings
Connect the USB to TTL converter to FRDM-MCXC242 board. FRDM-MCXC242 UART pins:
TX of USB2COM to J1-5
RX of USB2COM to J1-7
GND of USB2COM to J2-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Connect the USB to TTL converter to PC host.
Open a serial terminal on PC for the USB to TTL converter with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the UART Terminal port which connected to the USB2COM like:
USART DMA example
Send back received data
Echo every 8 characters
When you input 8 characters, system will echo it by UART and them would be seen on the OpenSDA terminal.