Hardware requirements
USB-C cable
FRDM-MCXC242 board
Personal Computer
Board settings
The flexio_i2c_read_accel_value example is requires connecting the FLEXIO pins with the I2C pins of accelerometer But this example no need special setting because of default FlexIO pins using is match with I2C pins of accelerometor on board.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
FlexIO I2C example read accelerometer value
Found an FXOS8700 on board, the device address is 0x1D .
The accel values:
status_reg = 0xff , x = -21 , y = 12 , z = 2007
status_reg = 0xff , x = -20 , y = 20 , z = 2008
status_reg = 0xff , x = -19 , y = 4 , z = 2008
status_reg = 0xff , x = -20 , y = 29 , z = 2022
status_reg = 0xff , x = -22 , y = 11 , z = 2008
status_reg = 0xff , x = -18 , y = 33 , z = 2013
status_reg = 0xff , x = -28 , y = 21 , z = 2005
status_reg = 0xff , x = -16 , y = 30 , z = 2022
status_reg = 0xff , x = -29 , y = 13 , z = 2010
status_reg = 0xff , x = -14 , y = 6 , z = 2024
End of FlexIO I2C example .