Hardware requirements
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
ADC LOW POWER ASYNC DMA DEMO
ADC16_DoAutoCalibration() Done.
ADC Full Range: 65536
Please press any key to trigger ADC conversion.
ADC value: 15670
Please press any key to trigger ADC conversion.
ADC value: 16634
Please press any key to trigger ADC conversion.
ADC value: 16686
Please press any key to trigger ADC conversion.
ADC value: 16681
Please press any key to trigger ADC conversion.
Note:
LED will be toggled when the CPU wake up.