Hardware requirements
Type-C USB cable
FRDM-MCXE247 Board
Personal Computer
Board settings
The example requires 2 boards.
Board to board connections needed to be as follows:
Node A connect to Node B
Pin Name Board Location Pin Name Board Location
CANH J16-1 CANH J16-1
CANL J16-2 CANL J16-2
GND J16-4 GND J16-4
Prepare the Demo
Connect the type-C USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
After connecting the two boards, these instructions display on each terminal window. One board must be chosen as node A and the other board as node B. (Note: Node B should start first) Data is sent continuously between the node A and the node B.
This message displays on the node A terminal:
FlexCAN pretended networking wake up example.
Please select local node as A or B:
Note: Node B should start first.
Node:a
Press any key to trigger one-shot transmission
Send message ID: 0x123, payload: 0x0055000000000000
Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0155000000000000
Press any key to trigger the next transmission!
Send message ID: 0x125, payload: 0x0255000000000000
Press any key to trigger the next transmission!
Send message ID: 0x125, payload: 0x0355000000000000
Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0455000000000000
Press any key to trigger the next transmission!
Send message ID: 0x123, payload: 0x0056000000000000
...
This message displays on the node B terminal:
FlexCAN pretended networking wake up example. Please select local node as A or B: Note: Node B should start first. Node:b Note B will enter lower power mode and wake up until received 4 specific messages. Wake up message format: Standard (11 bit id) Wake up message ID range: 0x123 to 0x124 Wake up payload range : 0x0055000000000000 to 0x0056000000000000 Waken up! Match message 0 ID: 0x123, payload: 0x0055000000000000 Match message 1 ID: 0x123, payload: 0x0155000000000000 Match message 2 ID: 0x123, payload: 0x0455000000000000 Match message 3 ID: 0x123, payload: 0x0056000000000000 Enter lower power mode again!