Hardware requirements
USB-C cable
Two FRDM-MCXE247 boards
Personal Computer
Board settings
SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board
INSTANCE0(SPI0) CONNECTS TO INSTANCE0(SPI0)
Pin Name Board Location Pin Name Board Location
SOUT J6 pin 6 SIN J6 pin 5
SIN J6 pin 5 SOUT J6 pin 6
SCK J6 pin 4 SCK J6 pin 4
PCS2 J6 pin 3 PCS2 J6 pin 3
GND J6 pin 8 GND J6 pin 8
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.