Hardware requirements
Type-C USB cable
FRDM-MCXE318 board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
BCTU SoftWare Trigger Example
Please press any key to get the ADC value
ADC channel 48 value: 12021
ADC channel 48 value: 12019
ADC channel 48 value: 12022