Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
LCD-PAR-S035 board
Board settings
Connect the LCD panel to header J8.
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the project running, the panel shows as overview described.