Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings
LPI2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of LPI2C interface, LPI2C_1 pins of MASTER_BOARD are connected with LPI2C_1 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
LPI2C_1_SCL J2-20 LPI2C_1_SCL J2-20
LPI2C_1_SDA J2-18 LPI2C_1_SDA J2-18
GND J2-14 GND J2-14
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C board2board polling example -- Master transfer.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
Receive sent data from slave :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .