Hardware requirements
Type-C USB cable
FRDM-MCXE31B board
Personal Computer
Board settings
LPSPI:
INSTANCE1(LPSPI_1) CONNECTS TO INSTANCE1(LPSPI_1)
Pin Name Board Location Pin Name Board Location
SOUT J6 pin 6 SIN J6 pin 5
SIN J6 pin 5 SOUT J6 pin 6
SCK J6 pin 4 SCK J6 pin 4
PCS0 J6 pin 3 PCS0 J6 pin 3
GND J6 pin 8 GND J6 pin 8
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for MCU-Link serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.