Hardware requirements
Type-C USB cable
FRDM-MCXN947 Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When running the demo, the debug console shows the menu to command the MCU to the target power mode.
NOTE: 1.Only input when the demo asks for input. Input entered at any other time might cause the debug console to overflow and receive the wrong input value. 2. Wake-up from Deep Power Down mode through wakeup reset that will reset the program(“Normal Boot” will be printed). 3. The signal output from J2_7 can be used to observe entry/exit of DeepSleep, PowerDown, and Deep Power Down mode.
Normal Boot.
########################### Power Mode Switch Demo ###########################
Core Clock = 48000000Hz
Power mode: Active
Select the desired operation
Press A to enter: Active mode
Press B to enter: Sleep mode
Press C to enter: DeepSleep mode
Press D to enter: PowerDown mode
Press E to enter: DeepPowerDown mode
Waiting for power mode select...