Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Note: Jumper setting:
MASTER connect to SLAVE
Pin Name Board Location Pin Name Board Location
SOUT J2 - 8 SIN J2 - 10
SIN J2 - 10 SOUT J2 - 8
SCK J2 - 12 SCK J2 - 12
PCS0 J2 - 6 PCS0 J2 - 6
GND J2 - 14 GND J2 - 14
Other jumpers keep default configuration.
Prepare the Demo
Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.
Open a serial terminal on PC for MCU-Link serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.