Hardware requirements

  • Type-C USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the hello world multicore demo in the terminal window:

Copy Secondary core image to address: 0x2004e000, size: 3280
Starting Secondary core.

Hello World from the Primary Core!

Starting Secondary core.
The secondary core application has been started.

Note: The “Copy Secondary core image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.