Hardware requirements
Mini/micro USB cable
RJ45 Network cable
FRDM-MCXN947 board
Personal Computer
Board settings
Board provisioning details
For board provisioning it’s best to use MCUXpresso Secure Provisioning tool.
Besides required setup the following settings need to be applied:
- Boot type set as “Signed”
- CFPA_PAGE_VERSION
set to at least 1 (non-zero and non-all-one)
- Flash swapping enabled; CMPA field FLASH_CFG.FLASH_REMAP_SIZE
set to 0b11111
The Dual image boot option allows to select for which slot (slot0/slot1) the SB3 file is being created. To create SB3 file used for an update, the target image should be set as “Image 1” - this reflects the process of using the second dormant slot as a space for the new image. It’s important to realize that with Flash Swapping enabled the ROM selects an image with higher Image version. If higher version image is located in the second slot (offset 0x100000) it swaps the slot0/slot1 addresses making it effectively appear at the beginning of the flash (offset 0). Therefore also make sure that Image version of the new image is higher than the currently installed one.