Hardware requirements
Type-C USB cable
FRDM-MCXW23 Board
Personal Computer
Board settings
MASTER_BOARD(I2C1) CONNECTS TO SLAVE_BOARD(I2C2)
Pin Name Board Location Pin Name Board Location
I2C_SCL J2-1 I2C_SCL J2-6
I2C_SDA J2-2 I2C_SDA J2-7
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
==FreeRTOS I2C example start.==
This example use one i2c instance as master and another as slave on one board.
Master will send data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
I2C slave transfer completed successfully.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
This time , slave will send data: :
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
Master received data :
0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8
0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0
0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8
0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0
End of FreeRTOS I2C example.