Hardware requirements
Type-C USB cable
FRDM-MCXW71 Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
MASTER(FlexIO SPI) connect to SLAVE(FlexIO SPI)
Pin Name Board Location Pin Name Board Location
SOUT J1 pin 3 SIN J1 pin 3
SIN J1 pin 2 SOUT J1 pin 2
SCK J1 pin 4 SCK J1 pin 4
PCS0 J1 pin 1 PCS0 J1 pin 1
Prepare the Demo
Connect a USB cable between the host PC and the FRDM board J10.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
FlexIO SPI edma example
Master Start...
Master runs successfully!