Hardware requirements
Micro USB cable
FRDM-RW612 board
Personal Computer
Board settings
I2C one board:
Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C2 pins of MASTER_BOARD are connected with I2C2 pins of SLAVE_BOARD
MASTER_BOARD CONNECTS TO SLAVE_BOARD
Pin Name Board Location Pin Name Board Location
GPIO_16 J2-18 GPIO_16 J2-18
GPIO_17 J2-20 GPIO_17 J2-20
GND J2-14 GND J2-14
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
The following message shows in the terminal if the example runs successfully.
CMSIS I2C board2board interrupt example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of I2C example .