Hardware requirements
Micro USB cable
IMX943-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
LCD SPEC panel
Board settings
Connect the LCD SPEC panel to J38
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW1(SYS_PWR) to power on the board.
Connect a micro USB cable between the host PC and the J15(FTDI_DEBUG) USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs, the screen shows what described in overview. The log below shows the output of the demo in the terminal window:
PXP Color Key example start...