Hardware requirements
Type-C USB cable
IMX95LPD5-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Populate R966 and R967 to establish connection between FLEXIO1(as master) and LPI2C6(as slave).
HAL_PINCTRL_PLATFORM_IOMUXC_PAD_GPIO_IO09__FLEXIO1_FLEXIO_BIT9 , HAL_PINCTRL_PLATFORM_IOMUXC_PAD_GPIO_IO03__LPI2C6_SCL connected
HAL_PINCTRL_PLATFORM_IOMUXC_PAD_GPIO_IO08__FLEXIO1_FLEXIO_BIT8 , HAL_PINCTRL_PLATFORM_IOMUXC_PAD_GPIO_IO02__LPI2C6_SDA connected
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
FlexIO I2C interrupt - LPI2C interrupt
Master will send data :
0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07
0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F
Slave received data :
0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07
0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F