Hardware requirements
Personal Computer
IMX95LPD5BB-19-REV-A EVK board
12V~20V power supply
J-Link Debug Probe
Micro USB cable
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect the 12V~20V power supply and J-Link Debug Probe to the board, and switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you will see similar information from the terminal shown below.
ADC sample rate measurement demo.
Please press any key to get the ADC sample rate.
Adc sample rate: 1002000 sps.
Please press any key to get the ADC sample rate.
Adc sample rate: 1002000 sps.
Please press any key to get the ADC sample rate.
Adc sample rate: 1002000 sps.