Hardware requirements
Personal Computer
IMX95VERDINEVK board
12V~20V power supply
J-Link Debug Probe
Micro USB cable
Board settings
Use the jumper to connect the J28 1-2, 3-4, 5-6
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect the 12V~20V power supply and J-Link Debug Probe to the board, and switch S6 to power on the board.
Connect a micro USB cable between the host PC and the J4 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you will see similar information from the terminal shown below.
ADC polling example.
Please press any key to get the conversion result.
The channel 0 ADC conversion data is 4084.
The channel 1 ADC conversion data is 3740.
The channel 2 ADC conversion data is 2049.
Please press any key to get the conversion result.
The channel 0 ADC conversion data is 4085.
The channel 1 ADC conversion data is 3741.
The channel 2 ADC conversion data is 2049.
Please press any key to get the conversion result.
The channel 0 ADC conversion data is 4084.
The channel 1 ADC conversion data is 3739.
The channel 2 ADC conversion data is 2049.