Hardware requirements
Micro USB cable
LPC845 Breakout board
Personal Computer
Board settings
No special settings are required.
Prepare the demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
PINT Pattern Match example
PINT Pattern match events are configured
Press corresponding switches to generate events
This example configures “Pin Interrupt 0” to be invoked when K1 is pressed by the user. Bit slice 0 is configured as an endpoint in sticky falling edge mode. The interrupt callback prints
"PINT Pin Interrupt 0 event detected. PatternMatch status = 1".
“Pin Interrupt 2” is configured to be invoked when K3 is pressed. The interrupt callback prints
"PINT Pin Interrupt 2 event detected. PatternMatch status = 100".