Hardware requirements
Micro USB cable
LPCXpresso51U68 board
Personal Computer
Board settings
Populate jumper JP3. Connect SPI5 pins to SPI3 pins:
Master - SPI5 CONNECTS TO Slave - SPI3
Pin Name Board Location Pin Name Board Location
MISO J1 pin 11 MISO J4 pin 3
MOSI J1 pin 13 MOSI J4 pin 2
SCK J2 pin 8 SCK J4 pin 4
PCS2 J1 pin 15 PCS2 J4 pin 7
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the CMSIS DAP terminal like:
SPI dma example start.
This example use one spi instance as master and another as slave on one board.
Please make sure you make the correct line connection. Basically, the connection is:
SPI_master -- SPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is SPI slave dma transfer completed callback.
This is SPI master dma transfer completed callback.
SPI transfer all data matched!