Hardware requirements
Micro USB cable
LPCXpresso54S018 board
Personal Computer
headphones with 3.5 mm stereo jack
source of sound (line output to 3.5 mm stereo jack)
Board settings
No special settings are required on LPCXpresso54S018 board.
Prepare the Demo
Connect headphones to Audio HP / Line-Out connector.
Connect source of sound(from PC or Smart phone) to Audio Line-In connector.
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
This demo is an external flash plain load demo, ROM will copy image in external flash to SRAMX to run:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
Headphones will play what is input into Audio Line-In. Terminal window will show:
Configure codec
Configure I2S
Setup digital loopback