Hardware requirements
Micro USB cable
LPCXpresso54S018 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
This demo is showing SPIFI flash erasing and writing and this demo should only run in SRAMX:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash. The log below shows example output of the spifi example in the terminal window:
SPIFI flash polling example started
All data written is correct!
SPIFI Polling example Finished!