Hardware requirements

  • Micro USB cable

  • Two LPCXpresso55S06 boards

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI master interface on board to other SPI interface on other board

    Master_board(SPI3)           Slave_board(SPI3)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J12   pin 2        MISO       J12   pin 2
MOSI       J12   pin 1        MOSI       J12   pin 1
SCK        J10   pin 16       SCK        J10   pin 16
SSEL0      J10   pin 14       SSEL0      J10   pin 14
GND        J9    pin 8        GND        J9    pin 8

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo

When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ Master Start…!

Succeed! ​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~