Hardware requirements
Micro USB cable
LPCXpresso55S16 board
Personal Computer
headphones with 3.5 mm stereo jack
source of sound (line output to 3.5 mm stereo jack)
Board settings
No special is needed.
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect headphones to Audio HP / Line-Out connector.
Connect source of sound(from PC or Smart phone) to Audio Line-In connector.
Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Multi-peripheral Test!
AUDIO Loopback started!
Headphones will play what is input into Audio Line-In connector.
Accelerometer: Found Accelerometer!
USB device HID mouse test
Plug-in the device, which is running mouse test, into the PC.A HID-compliant mouse is enumerated in the Device Manager.
The mouse arrow is moving on PC screen in the rectangular rotation.
Press the WAKEUP button, the red LED will flash. Press the ISP button, the blue LED will flash. Press the USER button, the green LED will constant on.