Hardware requirements
Micro USB cable
LPCXpresso55S16 board
Personal Computer
Board settings
Output signal Board location
SCT0_OUT2 J12-12
SCT0_OUT6 J12-14
The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J1) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output in the terminal window:
SCTimer example to use it in 16-bit mode
The example shows both 16-bit counters running and toggling an output periodically
Probe oscilloscope at J12_12(5HZ) and J12_14(2.5HZ) to see output signal.