Hardware requirements

  • Micro USB cable

  • Two LPCXpresso55S16 boards

  • Personal Computer

Board settings

SPI one board: Transfer data from SPI slave interface on board to other SPI interface on other board

    Master_board(SPI7)           Slave_board(SPI7)                          
Pin Name   Board Location     Pin Name   Board Location                     
MISO       J9    pin 11       MISO       J9    pin 11
MOSI       J9    pin 9        MOSI       J9    pin 9
SCK        J9    pin 13       SCK        J9    pin 13
SSEL1      J9    pin 2        SSEL1      J9    pin 2
GND        J9    pin 8        GND        J9    pin 8                      

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
===============
1.  Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.
2.  Open a serial terminal with the following settings:
    - 115200 baud rate
    - 8 data bits
    - No parity
    - One stop bit
    - No flow control
3.  Download the program to the target board.
4.  Reset the SoC and run the project.

Running the demo
===============
When the demo runs successfully, the log would be seen on the terminal like:

​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
SPI board to board interrupt slave example started!

SPI transfer finished!
​~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~