Hardware requirements

  • Micro USB cable

  • Two LPCXpresso55S36 boards

  • Personal Computer

Board settings

Short JP52 1-2.

MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C_SCL    J122-12            I2C_SCL    J122-12
I2C_SDA    J122-6             I2C_SDA    J122-6
GND        J92-14             GND        J92-14  

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the LPC-Link USB port (J1) on the board.

  2. Open a serial terminal on PC for JLink serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following message shows in the terminal if the example runs successfully.

CMSIS I2C board2board interrupt example -- Slave transfer.


Slave received data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f


End of I2C example .