Hardware requirements

  • Mini/micro USB cable

  • LPCXpresso55S36 board

  • Personal Computer

Board settings

DAC output pin: J12-4

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

  5. A multimeter may be used to measure the DAC output voltage (Connector J12-4).

Running the demo

When the demo runs successfully, the log would be seen on the debug console terminal like:

DAC buffer interrupt Example. Press any key to trigger the DAC… DAC next output: 200 DAC next output: 300 DAC next output: 400 DAC next output: 500 DAC next output: 600 DAC next output: 700 DAC next output: 800 DAC next output: 900

Then user can measure the DAC output pin to check responding voltage.